STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1400 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 552 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Error Updating STM32Cube IDE to latest version

Hi, I am trying to update my STM32Cube to the latest version using Help > Check for Updates, the update fails with the following error:Trying to update Cube V1.9.0 to the latest, running OSX 13.0. How do I fix this?I found another thread which sugges...

EPala2_0-1699904553713.png
EPala.2 by Senior
  • 3681 Views
  • 4 replies
  • 2 kudos

Build problem with fresh new git clone

HiI have this strange problem which manifest itself using headless build and also inside CubeID when I git clone my project for the first time.Build Settings : I have 4 custom build configuration. I also removed Debug and Release configurations that ...

TGUCL.1 by Associate III
  • 1412 Views
  • 0 replies
  • 0 kudos

Using a defined constant inside HAL_UART_Transmit

Hello,I'm using STM32 with STM32CubeIDEThis is my code:#define SOME_DATA 0x01 HAL_UART_Transmit ( & huart6 , SOME_DATA , 1 , 1000 ) ;The compiler issues the following warning :passing argument 2 of 'HAL_UART_Transmit' makes pointer from integer witho...

skon.1 by Senior
  • 9238 Views
  • 10 replies
  • 0 kudos

Audio not playing when using DF mini player

when I am running this code,the audio is not playing.I checked everything.The connection is completely fine as some sound is coming when I power up the nucleo.the audio files are named from 1 to 6.mp3.where is the problem then?? 

Priyaa_0-1699707747416.png Priyaa_1-1699707751494.png
Priyaa by Associate II
  • 3482 Views
  • 2 replies
  • 0 kudos