Skip to main content
HHich.1
Associate
July 24, 2023
Question

Change App start address in STM32F4 ( Bootloader USB + App)

  • July 24, 2023
  • 1 reply
  • 1381 views

Hello all,

I have a project using STM32F407 with 1MB of flash and it uses :

  • USB Bootloader project ( start address 0x8000000)
  • App project ( Start address  0x800C000)

I want to change the App start address to sector 4 ( 0x08010000)

From my understanding I have to change the following defines

 

In bootloader, tell the bootloader wher to find the app !

 

 

#define USBD_DFU_APP_DEFAULT_ADD 0x08010000U

 

In App, in its linker  (STM32F407VGTx_FLASH.ld)

 

FLASH (rx) : ORIGIN = 0x8010000, LENGTH = 720K

 

I tried the above settings but it didn't work ! App doesn't start

I read that I have to change vector table address aswell  system_stm32f4xx.c

So I added the offset of 16K 

 

 

#define VECT_TAB_OFFSET 0x4000

 

 
 
But this didn't work either,
 
Any solution for my basic issue ?
 
    This topic has been closed for replies.

    1 reply

    Pavel A.
    July 24, 2023

    Why 16K if the address is 0x8010000 ? This is 64K.