STM32CubeIDE (MCUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 1.16.1 released

STM32CubeIDE 1.16.1 was released on st.com as well as an in-tool update patch aligned with STM32CubeMX v6.12.1 that is available for download. Main issues fixed in this minor release: Fixed issue when install OpenSTLinux MP2 plugin from OpenSTLinux r...

STM32CubeIDE 1.16.0 released

STM32CubeIDE 1.16.0 was released today on st.com as well as an in-tool update patch. What is new in 1.16.0?Microcontroller and board lists aligned with STM32CubeMX v6.12.0 : STM32C0, STM32WB0 and STM32MP25XXAdded CMake support for multicontext projec...

SMT32CubeIDE continuously opens a DOS shell

Hi,I had this problem since today.When I open the program, a DOS shell opens continuously (every 5 seconds or so). The cursor changes context continuously and it is impossible to develop any applications.I have tried:1) search in update, and in setti...

Alvaruccio77_0-1732543495516.png

Resolved! cannot debug with CUBEIDE "Error: failed to erase memory"

hi i am having a problem with my stm32cubeide, specifically i cant connect to the stm32f407vgt6 microcontroller on my custom board, but when loading or erasing with cubeprog everything goes smoothly.i have tried cleaning my board, updating stlink to ...

Screenshot 2024-11-16 162113.png Screenshot 2024-11-16 162215.png
OWLchan by Associate III
  • 333 Views
  • 3 replies
  • 1 kudos

STM32CubeIDE 1.16.1 released

STM32CubeIDE 1.16.1 was released on st.com as well as an in-tool update patch aligned with STM32CubeMX v6.12.1 that is available for download. Main issues fixed in this minor release: Fixed issue when install OpenSTLinux MP2 plugin from OpenSTLinux r...

Resolved! A problem with '-fcyclomatic-complexity'

I'm using kali linux and the latest version of arm gcc available on arm website and the latest CubeIDE. When I first set everything up everything was working fine, but then I created an empty project for another MCU(STM32 G030F6P6) and got the follow...

rambo by Associate
  • 2699 Views
  • 2 replies
  • 1 kudos

STM32L496G-Disco Pin Configuration question

Hello,I am new to stm programming. I got a STM32L496G-DISCO board and I wanted to create a new project. When I try to configure the pins i have a lot of yellow triangle warning icons and some of the fields are purple which can not be changed. I don't...

AndreeaP31_0-1732472011140.png AndreeaP31_1-1732472076599.png