Ultra librarian creates erroneous symbols for STM32F4xxR2 in KiCAD 5 format
- November 22, 2024
- 2 replies
- 753 views
I have the latest and greatest CubeIDE v1.16t.1, confirmed with recent attempts to upgrade it. Recently I have been experimenting with the ultra librarian tool output in the IOC editor, which looks to be extremely useful. I have a project that uses an STM32F401RBTX, it was created by an earlier version of CubeIDE, but upgraded when I opened it.
I use KiCAD 5, and have been able to successfully create a symbol on a different project. However, the symbol that it creates for this one has two errors: first the pins are all located on top of each other, and second the poly lines have fractional positioning data that is rejected by the symbol parser. I have attempted to text edit out the fractions, but the pins appear to be stuck together and any attempt to relocate them with the symbol editor fails.
I cannot find any information about how to configure the librarian, is there an update or fix for this? Generated zip file is attached.