STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1554 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Where to find the gcc in STM32 directory? How (and in what place) is it correct to specify the path to gcc files? I changed the PATH for make and gcc separately

22:39:03 **** Incremental Build of configuration Debug for project c1 ****make all Building file: ../src/c1.cInvoking: Cross GCC Compilergcc -O0 -g3 -Wall -c -fmessage-length=0 -MMD -MP -MF"src/c1.d" -MT"src/c1.o" -o "src/c1.o" "../src/c1.c"c:/st/stm...

DM-SH by Associate II
  • 19497 Views
  • 11 replies
  • 0 kudos

How to add C source files to a project in a Cube IDE project

I'm no noob to the STM32, but I am to Cube IDE.I've added a new directory for my user code to separate it as much as possible from this dog's dinner of code that Cube auto config creates. I've created a new function, it's all correct, its prototype i...

DiBosco by Senior II
  • 48652 Views
  • 14 replies
  • 12 kudos

Resolved! Please update CubeIDE installation guide and rel. notes

The installation guide UM2563 hasn't been updated since 2022. Information about supported/tested Linux versions needs refresh.Also, in the release notes, if new Linux versions are validated, please add this information, it would be helpful.Regards,--...

Pavel A. by Super User
  • 1753 Views
  • 1 replies
  • 1 kudos

TouchgfxDesigner Unexpected error has happened

Stm32CubeIDE with TouchGFX, I am trying to design, but I am encountering the following error:Sorry - something unexpected has happened which caused an error to occur in the Designer. For more information, see the log file located at: C:\Users\ibrahim...

Resolved! Implementing Arduino into CubeIDE

I have already spent hours trying to get the Arduino library working in my CubeIDE (1.12.0 IDE; latest STM32duino; Firmware F3 1.11.4). I set up all the include paths, and changed the arduino stuff, to point to the CubeIDE generated files. I had some...

Tobe by Senior III
  • 8620 Views
  • 6 replies
  • 1 kudos

Resolved! Using timers as perodic software event trigger

Hello!! I'm a total newbie, so sorry for any mistakes, and I would like to ask for simple explanations as well.As title states, I would like to use a timer chosen from TIMx, not as an output on a pin, but rather for software only usage, to do an acti...

I2C Slave “Repeated Start�? Callback?

STM32F105, HCLK=72MHz, HAL Ver 1.1.8.0, SCL = 100KHzIs there a “Repeated Start�? HAL callback? I couldn’t find any direct reference but does the STM32 I2C peripheral know when this occurs and set a status bit somewhere?In my application, I can’t allo...

raymartin by Associate II
  • 3703 Views
  • 3 replies
  • 1 kudos