Skip to main content
PZamb.2
Associate III
November 22, 2023
Question

ST-LINK GDB server not work Reason: (0) Unknown.

  • November 22, 2023
  • 0 replies
  • 722 views

Hi

I have this problem again..:

C:\ST\STM32CubeIDE_1.13.2\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.stlink-gdb-server.win32_2.1.0.202305091550\tools\bin>C:\ST\STM32CubeIDE_1.13.2\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.stlink-gdb-server.win32_2.1.0.202305091550\tools\bin\ST-LINK_gdbserver.exe -p 61235 -l 1 -d -t -s -cp C:\ST\STM32CubeIDE_1.13.2\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.1.0.202305091550\tools\bin -el C:\workspace2\downloader_test\Debug\downloader_External_Flash.stldr -m 0 -k


STMicroelectronics ST-LINK GDB server. Version 7.4.0
Copyright (c) 2023, STMicroelectronics. All rights reserved.

Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61235
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled

Failed to bind to port 61236, error code -1: No such file or directory
Failure starting SWV server on TCP port: 61236
Failed to bind to port 61235, error code -1: No such file or directory
Failure starting GDB server: TCP port 61235 not available.
Shutting down...
Exit.

The ST-Link works with stm programmer but not work in stm32cubeide 1.13.2 (windows 11).

I try to unistall stm32cube ide anr reistall again but not change.

the hardware is custom board with stl-ink v2 usb programmer , wit the prevision version of cube was working without problem.

Reboot of pc not effect

someone have any suggest ?

    This topic has been closed for replies.