STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1554 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

ST-Link V2 usb drive error

I am currently trying to test my PCB that I made using the STM32F407VGT6 microcontroller. I have my code to toggle a led using a gpio output pin on the controller connected to the led on a breadboard. Under the system core on STM32IDE I have the SYS ...

keatonr by Associate
  • 1280 Views
  • 1 replies
  • 0 kudos

Not able to run FreeRtos task with trustZone enabled

Hi , I am trying to implement FreeRtos in my application with TrustZone enabled. I want to blink LED1 in task1 and LED2 in task2. Neither of the task are running. When I did the debugging in function xTaskCreate it's going into Infinite loop. My conf...

Kendall7_0-1711715069133.png
Kendall7 by Associate II
  • 3504 Views
  • 2 replies
  • 0 kudos

CubeMXIDE bug; EMDOS and Azure inclusions

This has been a long standing problem.If Azure is installed once (on this system), then for search paths in project properties, it is always present.If EmDOS has ever been tried, even though it is not selected and has been removed.  The EmDOS library...

Resolved! How to use DTCMRAM in stm32h743

Hi All,I want to use DTCRAM in stm32cubeide, the controller i used is stm32h743, earlier IUsed RAM_D2. shifting from RAM_D2 to DTCRAM is possible but both i cant use,please guide me, /DISCARD/ : { libc.a ( * ) libm.a ( * ) libgcc.a ( * ...

ykn by Senior
  • 11782 Views
  • 12 replies
  • 3 kudos

Resolved! variable gets undefined behaviour out of the loop body

Hi,I am writing C++ program on Visual Basic first, once it is compiled I will port it into STM32 Cube IDE environment. I wrote a simple for loop. When I run this code, I get very strange value for z out of the loop that is 1971940899.You can see the ...

demir by Senior II
  • 1380 Views
  • 1 replies
  • 1 kudos

Resolved! Facing Hard fault when implementing RTOS on NUCLEO-H563 board

Hi  I am trying to RTOS on my device STM32-H563ZI I get a hard fault when I hit the function osKernelStart(); in the main loop When I started debugging ,my code seems to get  hardfault after vStartFirstTask in function xPortStartScheduler() I am tryi...

Kendall7 by Associate II
  • 1589 Views
  • 1 replies
  • 0 kudos