STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1427 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 558 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! STM32H747 Touchgfx Custom Board Config

hi . I am trying to use a display lcd using parallel rgb (LTDC RGB888) with STM32h747XIH on a special board.STM32CUBE-IDE v1.14.0Touchgfx Designer  v4.22.1STM32Cube_FW_H7_V1.11.1My project creation steps are as follows :1-Stm32 project creation2-RCC ...

dsi.png xtouch.png
snnzdmr1 by Associate III
  • 3066 Views
  • 3 replies
  • 0 kudos

Do you trust these signers? Update 1.13.1

Hello Communitythe new update 1.13.1 just popped up. When I click throuhg the update process the following windows pops up: To be honest: this does not look very trustworthy. Even if "Legion of the Bouncy Castle" seems to be a legit certificate from ...

signers.png
CBerg by Senior II
  • 3886 Views
  • 4 replies
  • 2 kudos

Resolved! Errors in STM32CubeIDE firmware update offline.

Hi,I have a problem with STM32CubeIDE firmware update. STM32CubeIDE wants me to download stm32cube firmware f7_v1.16.0. I downloaded manually this update file offline because of the system have no internet connection. I moved the whole STM32CubeFW-F...

AK47 by Associate II
  • 13415 Views
  • 6 replies
  • 1 kudos

Resolved! ST-Link is not in the DFU mode, No ST-LINK detected!

Je suis incapable de déboguer le code sur ma carte STM32WLE5JC. STM32CubeIDE affiche un message d'erreur indiquant que le ST-Link n'est pas connecté. Cependant, le ST-Link est correctement détecté et connecté dans le STM32CubeProgrammer.

Capture d'écran 2024-03-22 123543.png Capture d'écran 2024-03-22 123943.png Capture d'écran 2024-03-22 124013.png

Resolved! CMake error when building STM32 project outside STM32CubeIde

Hello everybody,I'm trying to build an STM32 simple example based on CMake from the Windows shell but I got an error (I think because CMake doesn't find the GCC STM32CubeIde toolchain configuration).If I run CMake from STM32CubeIde all works fine (I ...

MaxC by Associate III
  • 6326 Views
  • 4 replies
  • 6 kudos