STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1406 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 556 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! [SOLVED] Unable to retrieve the count from TIM1 in Encoder Mode

Hi, I'm using an STM32F439ZI (on a nucleo board) and connected a Zaber stage with its encoder to it. When disconnected, I can measure the A & B signals schanging from GND to 5V. I currently cannot paste an image from the scope but I've lookerd at the...

debug_0-1712181677426.png
debug by Associate III
  • 1740 Views
  • 1 replies
  • 0 kudos

CAN1 communication doesnt work

Hi I'm very new in working with CAN-bus. My project involves two stm32 boards (both are nucleo-l433rc-p) and I want to get CAN-bus communication between them. The code is supposed to make a build in LED blink each time the blue button on the main nuc...

Mr4_1-1708681676633.png Mr4_2-1708681748704.png Mr4_3-1708681789418.png Mr4_4-1708681846276.png
Mr4 by Associate III
  • 1688 Views
  • 2 replies
  • 0 kudos

Resolved! build warning as cast to pointer from integer of different size

Hi,I am getting warning as build output as below. phaseBegin and phaseEnd is of type uint16_t. But, I typecast it as pointer variable to point uint8_t, because HAL_I2C_Mem_Read expects that argument to be pointer to uint8_t data.My code is here.Could...

demir by Senior II
  • 6371 Views
  • 1 replies
  • 2 kudos

Resolved! STM32CubeIDE Version: 1.15.0 Update and Login Problem

Hello The STM32CubeIDE Version: 1.15.0 doesn't create the code for me because I can't login in the software persistently can't connect to the internet. I followed some advice found on this community thread https://community.st.com/t5/stm32cubeide-mcu...

Cattura.PNG
AntoR by Associate III
  • 1300 Views
  • 2 replies
  • 2 kudos

Hardfault handler infinite loop

Hello, I am currently using a Nucleo F446RE board and i am facing problem while trying to read an analog pin using ADC functions. When i start running or debugging the project, i immediately fall down into Hardfault_handler function. I don't know wha...

Erwan03 by Associate III
  • 3942 Views
  • 5 replies
  • 1 kudos

Resolved! problem in compilations

Hello,I have imported existing project to cubt ide version 1.5.below is the problem i am facing.Problem running CDT Scanner Discovery provider com.st.stm32cube.ide.mcu.toolchain.armnone.setup.CrossBuiltinSpecsDetectorError serializing language settin...

vrund by Associate II
  • 3718 Views
  • 5 replies
  • 0 kudos

Resolved! API is not coming up outside of the function body

Hi,I am trying to add HAL_I2C_Mem_Read into my application. However, when I write the API in the region below, it is not auto filled, I can not use the API. On the other hand, when I add the API inside the above function it works.How can I fix this ?...

demir_0-1712148947715.png demir_1-1712148996290.png
demir by Senior II
  • 1892 Views
  • 3 replies
  • 1 kudos

Resolved! Undefined Reference

Hi,    I am using STM controller(STML031K6) first time and I have successfully run led program now I want to use timer (interrupt basis) but facing issues(undefined reference).      main.c /* USER CODE BEGIN Header */ /** ***************************...

vinaytiwary_0-1712145056456.png