STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1550 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Problem STM32CubeIDE update with stm32cube_fw_f7_v1161.zip

Hi,When I save modifications into Device Configuration Tool, the IDE do an update. It can't get the file stm32cube_fw_f7_v1161.zip, timeout.It's probably linked to my professional proxy configuration, but I can't resolved it currentlySomeone can help...

ABITT.1 by Associate III
  • 3023 Views
  • 4 replies
  • 0 kudos

Resolved! Optionally adjust the clock of the ADC

Hi I'm KIM from south Korea. My MCU is "STM32H735ZGT6". I want to change the clock of ADC1 within the code.I set up the clock of ADC1 in CUBEMX Clock Configuration about 80Mhz, but I want the clock of ADC1 about 75Mhz. How can I change the clock? Tha...

giwonKIM by Associate III
  • 2216 Views
  • 4 replies
  • 1 kudos

STM32CubeIDE CMake with Ninja???

Does anyone know how to coax cube IDE into wanting to use ninja as the build tool with a CMake project?  I’ve been away from cube IDE for a while but the allure of CMake and advanced debugging has sucked me back in again. I’m on MacOS and ninja is av...

svcguy by Associate III
  • 1714 Views
  • 0 replies
  • 2 kudos

error: launching debug has encountered a problem

Hello, I am trying to run a st demonstration (MEMSMIC1)  on stcubeIDE but i am getting an error within the debug, saying that the .elf file has failed to launch. How do I fix this? I am just trying to run the example as it is, I havent changed anythi...

Screenshot (25).png

Resolved! Can't Run from CubeIDE

Hi,Run from CubeIDE had not seen any issues until yesterday, but since then I can't run from CubeIDE, and don't know why.Download in CubeProgrammer is OK. I found if I do a mass erase on full chip in CubeProgrammer, then I can run once in CubeIDE. Th...

Chao_0-1713020029657.png
Chao by Senior II
  • 1756 Views
  • 2 replies
  • 0 kudos

Cant download any software

Dear support, I have tried to download STM32ide and STM32CubeMX, however anything i have tried pops up a window which says"This software is not available for download.". This happens on every tool i tried to download. At first I have though that this...

Screenshot 2024-04-16 at 12.57.19.png Screenshot 2024-04-16 at 12.53.49.png
vrezhMik by Associate
  • 3246 Views
  • 1 replies
  • 0 kudos

Resolved! Release build won't run

Hi all,I have a simple project using a STM32C011J4. Using STM32CubeIDE V1.15. I compile it for both Debug & Release.I program it via STM32Programmer V2.10.The Debug elf file works okay, however, the Release elf does NOT run…Yes! I have checked that t...

PGump.1 by Senior III
  • 14181 Views
  • 29 replies
  • 7 kudos

lsm303dlhc on kit STM32f411

Hi everybodyI am testing the LSM303DLHC sensor on the STM32f411 Discovery kit. The values ​​of the three axes x,y,z are 600, 4800, 15040 respectively. The values ​​of the three axes x,y,z change when I move the board.I don't know if the result is rig...

ThienNguyen0301_0-1713205001912.png ThienNguyen0301_1-1713205025258.png ThienNguyen0301_2-1713205040788.png ThienNguyen0301_3-1713205053484.png