STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1417 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 558 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Is RTOS CMSIS_V2 working with USB Host?

Hello,I tried to convert a test project that worked without RTOS, to use RTOS CMSIS_V2 and is not working with USB Host.I tried to convert a test project that worked without RTOS, to use RTOS CMSIS_V1 and is working with USB Host.Should I use CMSIS_V...

by Not applicable
  • 2094 Views
  • 3 replies
  • 0 kudos

Resolved! STM32F446RET SPI Problem With CC1120 Device

Im currently working on a custom PCB with cc1120 as transceiver and stm32f446RET6 as MCU. I integrate the cc1120 library from IT's library. The device uses SPI as serial communication. Here is the communication example in given datasheet. With this i...

Pasted image 20240424003521.png Pasted image 20240424003611.png Pasted image 20240424004458.png Pasted image 20240424005159.png
mrkayaalp by Associate III
  • 8811 Views
  • 17 replies
  • 5 kudos

what is ~/STM32Cube/Repository

During seeking for space on my macOS hard drive I found 12GB of files in~/STM32Cube/RepositoryWhere do they stem from? Can I delete them? Has it got to do sth. wit STM32CubeIDE? 

Resolved! I2C Not Working

Hello,I am trying to setup an external ADC/DAC module with an STM32H7 microcontroller. I2C Slave - EVAL-AD5593R-PMDZI2C Master - STM32H757XIH6 on STM32 Embedded Display by RiverdiI am struggling to get the very basics of communication to work as I ca...

Resolved! STM32 Cube IDE 1.15 USB Middleware Codegen Bug

Steps to reproduce:Create a new project with an STM32F779NIH processorEnable USB OTG highspeed (device only)Add USB_Device middleware (select any class)Generate the project codeInside the USB_DEVICE/App/usbd_desc.c file, the GetSerialNum(void) functi...

DrWidget by Associate II
  • 4302 Views
  • 6 replies
  • 4 kudos

can't open project if folder is already imported

I'm trying to open the example project "GPIO_InfiniteLedToggling". Apparently I did tis nce because I can't choose the project since "folder is already imported as project". If I choose (what I assume to be the created project) "GPIO_InfiniteLedToggl...

Jamiw by Associate II
  • 5098 Views
  • 5 replies
  • 0 kudos

Resolved! How to confirm firmware

I’m using STM32CubeIDE headless-build script in Linux for developing the software.I have a question regarding how to check the version of the firmware that I’m actually using in my environment.I tried to set a certain version of the firmware by writi...

u1kano by Associate III
  • 5022 Views
  • 7 replies
  • 0 kudos