STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1549 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

configuration

Hi,I now implementing i2c with 1 master (U575ZI-Q) and 3 slave (LK432KC).I confirmed my code. It worked well.but after changed title of the project and deleted some project, it made me confued,, so I made every(1master 3slave) project new. Here is th...

eunni_0-1714758042670.png eunni_1-1714758057098.png eunni_2-1714758125923.png eunni_3-1714758171256.png
eunni by Associate III
  • 6404 Views
  • 7 replies
  • 0 kudos

Resolved! Code Generation - USB OTG HS STM32H723ZGT6

Ran into a issue with a fresh blank project, only USB OTG HS turned on. Computer would recognize the usb device but as soon as I would turn any level of optimization on the computer would no longer detect the usb and show it as connected.  I was able...

stm32l051c8 standby mode

hi all currently i am working with stm32l051c8 , using that i can work with standby mode, its not entering to standby mode, can  u guide me any oneif (__HAL_PWR_GET_FLAG(PWR_FLAG_SB) != RESET){__HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB); // clear the flag /** ...

Resolved! STM32CubeIDE Library issues

Hello, I am trying to use the TensorFlow Lite Micro library for my project in STM32CubeIDE.I have made a folder for the library in my project as shown: I have included the directory for the folder in under the "Path and Symbols" tab:When I simply try...

mathieusteketee_0-1714264556733.png mathieusteketee_1-1714264745926.png mathieusteketee_2-1714264895949.png mathieusteketee_3-1714264973248.png

Resolved! Is it possible to load an array data while debugging?

Hello,I would like to know if is it possible to load an array data (from a text file or something like that) while debugging.Imagine to have the array int data[100];I would like to be able to fill it (while debugging) with values generated by me.Is t...

Nexum by Associate II
  • 2506 Views
  • 5 replies
  • 3 kudos