cancel
Showing results for 
Search instead for 
Did you mean: 

stm32l051c8 standby mode

sreedharan1196
Associate II

hi all currently i am working with stm32l051c8 , using that i can work with standby mode, its not entering to standby mode, can  u guide me any one

if (__HAL_PWR_GET_FLAG(PWR_FLAG_SB) != RESET)

{

__HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB); // clear the flag

 

/** display the string **/

char *str = "Wakeup from the STANDBY MODE\n\n";

 

HAL_UART_Transmit(&huart2, (uint8_t *)str, strlen (str), HAL_MAX_DELAY);

 

/** Disable the WWAKEUP PIN **/

HAL_PWR_DisableWakeUpPin(PWR_WAKEUP_PIN2); // disable PA0

 

}

 

/** Now enter the standby mode **/

 

/* Clear the WU FLAG */

__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);

/* Display the string */

char *str = "About to enter the STANDBY MODE\n\n";

 

HAL_UART_Transmit(&huart2, (uint8_t *)str, strlen (str), HAL_MAX_DELAY);

 

/* Enable the WAKEUP PIN */

HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN2);

 

/* one last string to be sure */

char *str2 = "STANDBY MODE is ON\n\n";

 

HAL_UART_Transmit(&huart2, (uint8_t *)str2, strlen (str2), HAL_MAX_DELAY);

 

/* Finally enter the standby mode */

HAL_PWR_EnterSTANDBYMode();

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0