STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1549 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

how to interface LoRa 993 with stm32f401RE

 Body:Hello STM community,I'm currently working on a project where I need to interface a LoRa 993 module with an STM32F401RE microcontroller. However, I'm encountering some issues, and I could use some guidance from those experienced in this area.I'v...

vinayak by Associate II
  • 5176 Views
  • 5 replies
  • 3 kudos

Working on STM32F030F4P6. Debugging is not supported

Hello everyone,I am new at working on STM32F030F4P6 this bord. I try to debug using ST-Link but was not abeal to use I also try  with OpenOCD but it stell not worked Spoiler  Image of the issueErrorSetings Is there any way to fix this 

Kai_Satone_0-1715145422964.png Kai_Satone_1-1715145453648.png Kai_Satone_2-1715145520959.png

Resolved! NUCLEO-G474RE Error in final launch sequence

I have successfully built the DRP1M1_DRP Dual-Role USB-C project targeting the NUCLEO-G474RE (supplied with X-CUBE-TCPP v4.4.0). The first time I tried RUN, I had to update the ST-LINK software on the NUCLEO board (it's brand new), but having done th...

alw by Senior
  • 6092 Views
  • 8 replies
  • 3 kudos

Can not download stmcube ide

recently if i going to download stmcube ide it says this software is not available for download can anyone help me regarding this?Thanks in Advance

Asraful by Associate III
  • 6622 Views
  • 10 replies
  • 1 kudos

Resolved! How to enable global interrupt for TIM3 (in PWM mode)

Hi, I want to enable the global interrupt for TIM3 so that I can recognize when it becimes active (it raises the pin).I've added:if(htim_base->Instance==TIM3){/* Peripheral clock enable */ __HAL_RCC_TIM3_CLK_ENABLE();/* TIM2 interrupt Init */HAL_NVIC...

debug by Associate III
  • 3218 Views
  • 2 replies
  • 2 kudos

Resolved! Remove CubeIDE editor margin TODO tags.

Does anyone know how to remove the tags that show in the margin to the left of the line numbers in the editor when you have a 'TODO' in a comment on the line? They inhibit my viewing of breakpoints on the line. I guess I could get rid of side comment...

jlag_1-1714693120799.png
jlag by Associate III
  • 3346 Views
  • 4 replies
  • 5 kudos