cancel
Showing results for 
Search instead for 
Did you mean: 

Ethernet peripheral Usage( Transmit and Recieve ) Without LwIP Stack on Nucleo-H743ZI2

khalinuxx
Associate

Hello all,

I am currently working on a project that involves utilizing the Ethernet peripheral on the Nucleo-H743ZI2 development board. While researching implementation options, I noticed that many resources recommend using the LwIP stack for handling Ethernet communication. However, for various reasons specific to my project requirements, I would prefer to avoid using the LwIP stack.

Could you please provide any resources, code examples on how to utilize the Ethernet peripheral with STM32Cube_FW_H7_V1.11.2 on the Nucleo-H743ZI2 board without relying on the LwIP stack? I am particularly interested in:

  1. Sending data packets over Ethernet.
  2. Receiving and processing incoming Ethernet packets with and without interrupt.
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Pavel A.
Super User

FreeRTOS, ThreadX/NetX and other RTOS work on STM32 and have their own network stack. Consider using these. 

Or roll your own network drivers even not based on TCP/IP.

However, there are no ready examples for the latter, you can use available LwIP examples or find a consultant.