User Activity

Hello,I can create a simple program in STM32CubeIDE V1.17.0 targeting the NUCLEO-G474RE board. I can build ok but am having problems with the GDB server starting. JP5 is set to 5V_USB_STLK and JP (BOOT0) is off. I can do the ST-Link Upgrade without p...
I have a NUCLEO-G491RE board connected to a PC running STM32CubeIDE v1.17.0. On first connection I was prompted to update the firmware on the board, which I did. On successful completion of the update I disconnected and reconnected the board, but the...
Is there a recommended minimum SMT package size and power rating for resistor R4 (8R2) please?
I am using TouchGFX Designer standalone and can build and simulate my project ok, but Program and Run Target fails with 'recipe for target '_extflash_' failed' even though STM32CubeProgrammer is connected to the STM32F7508-DK  board that I am using. ...
I created a project using the default port assignments for the STM32MP157D-DK1 board in STM32CubeIDE v1.16 and was able to build it successfully. Following the example of the STM32MP157 Workshop videos I used Device Tree Compiler to create .dtb files...