STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1540 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 586 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

BMA456 STM32

Hi, I have a project to finish where I have to use a bma456, which is a step counter sensor, on stm32CubeIde. But I can't seem to be able to do it, by running my own code or by using the code given on the git, I always seem to be stuck on the burst a...

dawlon by Associate
  • 3903 Views
  • 5 replies
  • 1 kudos

ADC using DMA

Hello, @mƎALLEm  I would like to measure the voltage on analog pin A0 and A1 simultaneously, using ADC in DMA mode. I configured my ADC settings as SCAN, CONTINUOUS mode to measure continuously the whole group. The DMA is also configured and linked t...

Erwan03 by Associate III
  • 1976 Views
  • 2 replies
  • 1 kudos

Resolved! DSP include files errors

I'm trying to implement the DSP functions, FFT...but including the "DSP include files" I get several errors: May you help me ? Thank you, Luigi

carloV_0-1717423305363.png
carloV by Associate III
  • 2618 Views
  • 4 replies
  • 0 kudos

ADC DMA

I am trying to capture input signal on the ADC using DMA and a Timer Interrupt.My board is STMH743VIHx.I am feeding an input sinusoidal signal to the ADC and,I am able to read values on DMA in a buffer. But I can't really understand the values I am g...

ssj16 by Associate
  • 1291 Views
  • 1 replies
  • 0 kudos

Resolved! Suddenly occured error

Hello,There was nothing wrong when I worked on it until yesterday.But when I went to work today and built it, an error like the picture appeared.I can't guess the cause at all.Reimporting the project or deleting the IDE and installing it anew does no...

스크린샷 2024-06-04 083632.png

Resolved! STM32H723 CMSIS DSP

Hi,I'm using a NUCLEO-H723ZG and I've installed the CMSIS DSP library, but when I try to compile the code something goes wrong... May you help me to understand what do I make wrong ? Thank you, Luigi

carloV_0-1717416140680.png
carloV by Associate III
  • 2806 Views
  • 2 replies
  • 0 kudos

Resolved! Debug inline assembler code

Hi,I have a inline assembly code to implement some math, like:************************************C-Code...asm(" push {%5};"" lsl %5, 1;"" add %5, %3;"...);C-Code*******************************************************Unfortunately I`m not able to ste...

berait by Associate III
  • 3063 Views
  • 3 replies
  • 0 kudos