STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1549 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 587 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

ST-LINK - Target no device found.

i am plugin the ST-link cable it shows COM6 in the devices but while debugging it is showing the below error Target no device found Error in initializing ST-LINK device.Reason: No device found on target. 

Import existing files into Cube project

Hi there,I used Rowley Crossstudio for STM32L011 development so far but wanted to try the CubeIDE as well.But upon generating a fresh STM32 project and importing my c++ files from my directory, I can't build the project because in the properties ther...

JohannesHofmann_0-1720292159156.png

Resolved! Missing definition of type "SPI_HandleTypeDef"

I have configured a STM32 project in the ioc interface to use SPI2 - I can see it having the green check mark in the ioc interface. However when I generate code I don't see any spi driver header, and when compiling I get a:error: unknown type name 'S...

slai-nick by Associate II
  • 4331 Views
  • 4 replies
  • 2 kudos

change the update period of the live expression view

Hello,I will debug a application on the STM32G030F6 which are use to 90% the low poer sleep mode. For this I will show the changes of variables in RAM and Flash also the changes of SFR from the MCU hardware like SPI in real time. I will also manipula...

bm2 by Associate III
  • 1938 Views
  • 2 replies
  • 0 kudos

Can't install STM32CubeIDE in Ubuntu 23

Getting the below error while installing The following packages have unmet dependencies: st-stm32cubeide-1.12.1 : Depends: libpython2.7 but it is not installableE: Unable to correct problems, you have held broken packages.

Raees by Associate III
  • 15818 Views
  • 10 replies
  • 18 kudos

How can I change UI size in .ioc file view?

Hello community!!I'm using Ubuntu 22.04 with 4k monitor and my fractional scaling set to 175%, and this is what I get in STM32CubeIDE .ioc file view, which is too small to read.I tried toggling some font settings in Window > Appearance, but didn't wo...

AO7_0-1712289415455.png
AO7 by Associate
  • 4012 Views
  • 4 replies
  • 5 kudos

Resolved! Can't debug - no such file or directory

Hello,I recently bought a NUCLEO-F412ZG and shortly downloaded STM32CubeIDE.However, I only tried to debug and launch the generated program, without changing anything, and came across this error message :Checked the path, all is good. I can't seem to...

leamrl_0-1720533244736.png
leamrl by Associate
  • 3139 Views
  • 3 replies
  • 5 kudos