STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1549 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 587 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

How to write the ADC value in stm32f103

Hello Everyone ,Im KarthikI need one help:Im working in stm32 CUBE IDE Read the ADC value in A0 my code is working but I cant able to Write the adc value .This is my Code:/* USER CODE BEGIN Header */ /** ********************************************...

USBPD for B-U585I-IOT02A

Hello forum,Im trying to create a code for reading from and writing to a USB flash drive using the USB-C connector,While activating the USBPD, USBX, TCPP, and FileX, the code generated missing some defines and variables like "DPM_Ports", "PWR_Port_PD...

Analog watchdog configuration bug

Hi,I have a project on Nucleo board with STM32U575ZIT6Q. I'm using STM32CubeIDE version 1.16.0 and CubeMX version 6.12.0. My .c and .h files are generated separately per peripheral.I was faced with an issue that watchdog works only with one channel.M...

aw.PNG conf.PNG ch.PNG
S-E by Associate II
  • 3624 Views
  • 7 replies
  • 1 kudos

USB CDC Transmit Hangs Intermittently

Using CDC USB on STM32G4 FW version 1.5.2, Win10 with default VCP driver.When calling CDC_Transmit_FS() from main() it will work for a few seconds and then hang indefinitely when TxState is never reset to 0. Others have had this issue (see: here, her...

eot105_0-1710777165869.png
eot105 by Associate
  • 1751 Views
  • 2 replies
  • 0 kudos

Resolved! USB Device Code Generation for STM32CubeIDE Version: 1.14.1

Hello,I am trying to create a HID device using the USB Device code generation in STM32CubeIDE Version: 1.14.1.But I have a problem with my PC not recognizing it as a HID device.MxCube.Version=6.5.0 is working fine and we have investigated the differe...

forst by Associate III
  • 1705 Views
  • 1 replies
  • 1 kudos