STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1467 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 570 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! HAL_Delay in uart receive interrupt

Hi When HAL_Delay goes into uart interrupt, the program stops. Is there a way to work it out?  I tried to use NVIC, but I don't know how to set it up.  Please advise. Thank you. Here is my uart interrupt service routine. void HAL_UART_RxCpltCallback(...

giwonKIM by Associate III
  • 2418 Views
  • 4 replies
  • 3 kudos

Resolved! 4 7-Segment Display multiplexing without driver

Hello, So, I'm trying to display a 4 Digit number on 4 7-segment Display using multiplexing The issues are - 1. I'm using different Ports for Segments and Different Ports For common Cathode Pins ( I'll add the code below)                           2....

Omkar23 by Associate II
  • 10573 Views
  • 6 replies
  • 6 kudos

Debugging Issue with STM32CubeIDE

Hello,I am encountering an issue while debugging a project using STM32CubeIDE. The problem arises when I start the debugging process. Below is the output from the console:Open On-Chip Debugger 0.12.0+dev-00597-ga5a21219f (2024-06-03-11:04) Licensed u...

romi by Associate III
  • 2509 Views
  • 1 replies
  • 0 kudos

Resolved! No capture IT triggered

Hi,Something seems to be wrong with STMCubeIDE Version: 1.16.0 Build: 21983_20240628_1741 (UTC) with an STM32G070RBT6. After generation of the code, the Timer code is like this:/*** @brief TIM3 Initialization Function* @param None* @retval None*/stat...

Gaetan by Associate
  • 1693 Views
  • 2 replies
  • 1 kudos

Code Coverage Gcov Lcov

Hello,is anyone able to generate a lcov coverage report in Stm32cubeIde or to visualize the the coverage result inside the editor?I have the *.gcno and *.gcda file (by semihosting). Regards Peter

PPete by Associate III
  • 2222 Views
  • 1 replies
  • 0 kudos

Resolved! Bad code generation with ADC LL API and STM32CubeIDE

I recently changed the configuration of working product from HAL API to LL API to improve performances.Unfortunately, the LL initialisation code generated by the STM32CubeIDE for the ADC was incomplete, and forgets to set the PCSEL register when need...

cberg.1 by Associate II
  • 2343 Views
  • 3 replies
  • 0 kudos