STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1532 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 584 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! FreeRtos error in STM32H7

  Hello, I am working with stm32H755 and FreeRTOS. After setting up debugger, I start debugging the program. the code is built fine, then get this error msg(attached picture) only if i enable FreeRTOS from the setup window(attached picture) . But i n...

image.png Screenshot 2024-10-02 140133.png
sazzad07 by Associate II
  • 3653 Views
  • 5 replies
  • 1 kudos

Resolved! STM32U073 - I2C

In documentation (RM0503), I2C CR1 register contains SBC bit field (Slave Byte Control), at position 16. Unfortunatelly, LL driver files (actually stm32u073xx.h, which is referred by driver files) have no corresponding defines.

Resolved! ADC not working properly on Nucleo-MB1549

I'm trying to get some adc values from my nucle-mb1549-ws but no matter what i do, i can't seem to get any values. Below i have attached the main.c file source code. Below is an image of my .ioc file to give you an idea of what is happening. I am try...

BadEngineer_0-1728402239296.png BadEngineer_1-1728402380161.png

Problem installing STM32CubeIDE on Debian Bookworm

Hi,I recently downloaded the general Linux install package en.st-stm32cubeide_1.16.1_22882_20240916_0822_amd64.sh.zip from https://www.st.com/en/development-tools/stm32cubeide.html.Using Ark, this was extracted into subfolder ~/Downloads/en.st-stm32c...

Resolved! Dependencies issue when installing STM32CubeCLT v16.0.0

Hi,I have a Ubuntu 24.04.1 LTS server running on AWS. I want to setup this server as my firmware build server. I was trying to install STM32CubeCLT v16.0.0 on the server but I am getting this output:    ubuntu@build_server:~$ sudo ./st-stm32cubeclt_1...

SBhon.1 by Associate III
  • 5119 Views
  • 1 replies
  • 0 kudos

Resolved! doesn't work GPIO_EXTI in original project

Hello,I made a GPIO_EXTI test project referring to GPIO_EXTI sample.For just check, I added entering Stop Mode int the GPIO_EXTI sample and HAL_GPIO_EXTI_Callback worked regularly like following. HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_ST...

curiae by Associate III
  • 2373 Views
  • 6 replies
  • 0 kudos

Resolved! ADC STM32H745

Hello team,I am using adc pins to detect voltage. In cube IDE I do adjustment to get ADC clock as 75MHz. But in the datasheet it is mentioned that for that package max adc clock is 50Mhz. Still cubeIDE(in .ioc file) does not shows any error and compi...

forum1.jpg forum2.jpg

ITM Debug with SWV H755

I am unable to get ITM debug working via either CubeIDE or Cube programmer.  I have checked the sysclock matches the sysclock configured for the system.I have tried various limits and auto for the SWV clock.I have enabled SWV in the debugger config.I...

tstokes_0-1728309818225.png tstokes_1-1728309947212.png
tstokes by Associate III
  • 1756 Views
  • 2 replies
  • 0 kudos