STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1249 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 512 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

CubeIDE v1.19 and v2.0.0 - very high CPU usage on Linux

Good morning.Using CubeIDE both v1.19 and v2.0.0 with Debian Linux v11.11.I'm seeing very high processor usage, 300% and higher, all of it java based even when there is no activity in the IDE.  Is there an explanation available for this usage, or is ...

SysMonitor.png
TJM by Senior II
  • 267 Views
  • 4 replies
  • 0 kudos

Jumping to random file after pressing Run button

Hello. When I press to Run (Run main.c) button, STM32CubeIDE opens random file, possibly, from current repository, for example: startup_stm32l452xx.s, core_cm4.h etc... Code is loading successful, but this side effect bothers me. I would like to dis...

GeneralTao by Associate II
  • 100722 Views
  • 230 replies
  • 133 kudos

STM32CubeIDE 1.14.0 pattern recipe problem

Hi,I have project for STM32F405 created manually. Project is using fixed GCC 4.92014q4.After updating STM32CubeIDE to version 1.14.0 i got warnings shown below.Compiler option "Cyclomatic Complexity" is disabled.File "subdir.mk" contains this rule:# ...

s1.png