2026-03-03 10:55 PM
During debugging its showing pop_up notification like Failed to enable live expression, connection failed but when i am click ok, after that its start downloading. what could be the reason for that one.
2026-03-03 11:34 PM
Hello @swathi_123
Are you using Jlink? it seems to be the same issue here Live expression do not work after upgrade to STM32... - Page 2 - STMicroelectronics Community
BR,
Souhaib
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.