STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1441 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 565 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! StmCube Ide 1.16 cannot use for debugging STM32L5

I just try using Nucleo L522ZE-Q and compile example codeafter i debug it, somehow it cannot write the file to the flashand the trace is not set properlyafter i downgrade the IDE using 1.14 it can work properly noplease fix the new IDE, i didn't want...

Azwar by Associate
  • 1303 Views
  • 2 replies
  • 0 kudos

Resolved! SPI configuration

Good morning,I'm new to using the STM32. I have a Nucleo H755ZI-Q development kit.I need to write a command to SPI port type 0xfcd8000 or 0xfcb85b0 or 0x12000000. The max frame can be 32 bits.On the oscilloscope, I do have an SPI frame, but I always ...

Gregory_1_0-1730891175976.png

Resolved! STM32CubeIDE - STM32U5 Port G Issue

Using STM32CubeIDE Version 1.14.1MCU Package STM32U5 1.4.0Using custom  STM32U5A9ZJT6Q  PCBIssue:-a.) if (HAL_GPIO_ReadPin(GPIOG, GPIO_PIN_7)) // PG7 pin 92 is always reading 0b.) HAL_GPIO_TogglePin(GPIOG, GPIO_PIN_12); // is not toggling the pinPort...

Resolved! J-LINK SEGGER with STM32CubeIDE

Hello, I would like to know How to configure the J-LINK Segger to work with STM32CubeIDE, after a little searching I found this video : https://www.youtube.com/watch?v=Rf-NKOoPYUc But at 12:11 I can see this configuration in the video              Bu...

DYann1_0-1730723182830.png DYann1_1-1730723371353.png
DYann.1 by Senior II
  • 20282 Views
  • 38 replies
  • 5 kudos