Skip to main content
Visitor II
July 1, 2024
Question

Target selection: STM32 target or STM32Cube example selection is required

  • July 1, 2024
  • 1 reply
  • 1038 views

When i try to create a STM32 project on Cubeide (wayland) i've been getting this error and can't select any board. I can't even see the Window to select board/mcu etc.

 

I've also tried to use it with Xorg and it's worse. The application crashes after a few seconds of pushing create stm32 project.

 

I've checked 14.0, 15.0 and 15.1 none of them working. Is stm32cubeide for linux broken?

    This topic has been closed for replies.

    1 reply

    Associate II
    July 16, 2024

    I'm getting the same problem on Window10.

    This is at the top of the screen

    decook1110_0-1721093561995.png

    And as you can see below, there are no boards to be selected from.

    decook1110_1-1721093666132.png

     If I go back to the select by MCU/MPU instead of by board and already know what specific board I want, I can then click on the board as an option.

    Also this only happens when I try to start a new project from inside STM32CubeIDE.   When I open CubeMX directly, the board selection tool works properly.

    I know the work around for this, but is there a fix, what should I be reloading?