cancel
Showing results for 
Search instead for 
Did you mean: 

Debug NUCLEO-L552ZE-Q

swenets
Associate

How can I download my application onto board when debugging from the Cube IDE 1.16 ?

I have the NUCLEO-L552ZE-Q, and using the Cube programmer I can program the .elf to flash as it seems, which takes like 30 seconds.

When I debug from the Cube IDE 1.16 it takes very short time and I see no dowloading of my .elf. 

How can I download my application automatically when going to debug.

2 REPLIES 2
Andrew Neil
Super User

It should do the download when you press the 'Debug' button, but you're not the first today saying that it doesn't:

https://community.st.com/t5/stm32cubeide-mcus/stm32cubeide-doesn-t-flash-target-before-debugging/td-p/697397

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Thanks Andrew,

It starts working w. 1.15.1.

-sten