STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1526 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 579 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Ubuntu 22.04 CubeIDE either freezing or no IOC editor

I was having this problem https://community.st.com/t5/stm32cubeide-mcus/stm32cubeide-user-interface-freezing-in-ubuntu-22-04-wayland/td-p/656993 so I tried the solution and it fixed the freezing, but now the IOC editor doesn't render, such as with ht...

DShekter by Associate III
  • 2183 Views
  • 5 replies
  • 1 kudos

STM32CubeIDE 1.14.1 Login to myST does nothing

With STM32CubeIDE 1.14.1 running on Windows10 the login to myST does not work anymore. Clicking the menu item or using the hotkey Alt-L simply does nothing - no reaction, no error message, NOTHING. It worked some time ago but all of a sudden does not...

MSchm.1 by Associate II
  • 8432 Views
  • 17 replies
  • 3 kudos

Is there support for github copilot?

Hi,I cannot find any information about the possibility to use github copilot in the STM32CubeIDE. Is it available or are there any plans to support it in the future?Or do you recommend using it in VS only?Thanks you for your answer

Hueli.1 by Associate III
  • 11769 Views
  • 7 replies
  • 12 kudos

STM32F439ZI TCP COMMUNICATION

I am a beginner in ethernet TCP protocol. I wanted to establish tcp connection between host and target(stm32f439zi). I don't know how to find ip address of an ethernet port connected in stm32.Can anyone help me to learn from basics and develop code a...

arun27 by Associate II
  • 1095 Views
  • 2 replies
  • 1 kudos

Resolved! STM32CubeIDE line command build on Windows

Hello,Does someone know where to find documentation on how to launch build using STM32CubeIDE line command on Windows?To specify my need, I have the command below and I would like to add an argument to redirect build log to a custom file :stm32cubeid...

HABIJ.1 by Associate III
  • 2498 Views
  • 4 replies
  • 1 kudos

Resolved! H5 ADC clock

Hi, I'm using the Cube IDE 1.17 on an H5.  The HCLK is 248MHz.  When I try to configure the ADC/DAC clock to use HCLK, I get a red error.  According to the data sheet, the maximum clock to the ADC is 75MHz.  I am configuring the clock as divide by 6....

Ubuntu 22.04.4 LTS STM32 Cube IDE installation errors

Hello ST,   I downloaded the latest cube IDE v1.16 Debian Linux Installer from the official link, performed the following steps: 1. Extract the zip.      sudo unzip en.st-stm32cubeide_1.16.0_21983_20240628_1741_amd64.deb_bundle.sh.zip     2. Change p...

pawanST by Associate
  • 3631 Views
  • 4 replies
  • 2 kudos