cancel
Showing results for 
Search instead for 
Did you mean: 

Ubuntu 22.04.4 LTS STM32 Cube IDE installation errors

pawanST
Associate

Hello ST,

 

I downloaded the latest cube IDE v1.16 Debian Linux Installer from the official link, performed the following steps:

1. Extract the zip. 

 

 

sudo unzip en.st-stm32cubeide_1.16.0_21983_20240628_1741_amd64.deb_bundle.sh.zip

 

 

2. Change permissions to run the extracted shell script

 

 

sudo chmod +x st-stm32cubeide_1.16.0_21983_20240628_1741_amd64.deb_bundle.sh

 

 

3. run the shell script

 

 

sudo ./st-stm32cubeide_1.16.0_21983_20240628_1741_amd64.deb_bundle.sh

 

 

I am stuck with the installation after accepting permissions please check the log below:

 

 

I ACCEPT (y) / I DO NOT ACCEPT (N) [N/y] y                                           
License accepted.
Reading package lists... Done
Building dependency tree... Done
Reading state information... Done
Note, selecting 'segger-jlink-udev-rules' instead of './segger-jlink-udev-rules-7.96j-linux-all.deb'
The following NEW packages will be installed:
  segger-jlink-udev-rules
0 upgraded, 1 newly installed, 0 to remove and 36 not upgraded.
Need to get 0 B/18.0 kB of archives.
After this operation, 0 B of additional disk space will be used.
Get:1 /home/gp/Downloads/makeself_dir_1PdcaK/segger-jlink-udev-rules-7.96j-linux-all.deb segger-jlink-udev-rules all 7.96j [18.0 kB]
(Reading database ... 282777 files and directories currently installed.)
Preparing to unpack .../segger-jlink-udev-rules-7.96j-linux-all.deb ...
Unpacking segger-jlink-udev-rules (7.96j) ...
dpkg: error processing archive /home/gp/Downloads/makeself_dir_1PdcaK/segger-jlink-udev-rules-7.96j-linux-all.deb (--unpack):
 trying to overwrite '/etc/udev/rules.d/99-jlink.rules', which is also in package jlink 7.963
Errors were encountered while processing:
 /home/gp/Downloads/makeself_dir_1PdcaK/segger-jlink-udev-rules-7.96j-linux-all.deb
N: Download is performed unsandboxed as root as file '/home/gp/Downloads/makeself_dir_1PdcaK/segger-jlink-udev-rules-7.96j-linux-all.deb' couldn't be accessed by user '_apt'. - pkgAcquire::Run (13: Permission denied)
E: Sub-process /usr/bin/dpkg returned an error code (1)

 

 

Please help me proceed further.

 

Thanks,

Pawan

4 REPLIES 4
Billy OWEN
ST Employee

Hi @pawanST 

 

This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

 

Regards,

Billy

Pavel A.
Super User

While waiting for solution from ST: the error is caused by installation of J-Link support, which is optional and may be not needed for you at all. Try to delete or rename the conflicting thing (/etc/udev/rules.d/99-jlink.rules)  before  installing CubeIDE. Or uninstall package jlink 7.963. Restore it later if needed.

 

Pavel, Thank you for the response. As you mentioned, I deleted the 99-jlink.rules but it did not improve the situation..

Will try more in similar lines. Thanks for the direction. 

@Billy OWEN , It's all right, if it is resolved, it will be helpful to everyone..

 

Thanks 

Pawan

 

 

 

Any updates on this topic?
Thanks