STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1526 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 580 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! STM32CUBEIDE code run extern flash

I'm using the STM32H7B0, but I want to place the executable file compiled from a certain file in the project into the external flash for execution. For example, the `BSP/led/led.c` file.I've modified the linker script (ld file), added the address of ...

Sunwaz by Associate III
  • 3323 Views
  • 5 replies
  • 0 kudos

Internet problems - PKIX path building failed...

Aftre installing STM32CubeIDE it fails to connect to internet - In Firmware Updater, "Check Connection" fails and does not give a reason. As extra test done "Check for Updates" and it also fails with error:PKIX path building failed: sun.security.prov...

NetView.png

Resolved! H7A3 - Code not loaded into ITCM-RAM

Hi all,i have an issue with an STM32-H7A3, which is going into hard fault, when calling a function, which is moved to the ITCM-RAM.I have defined a section for ITCM-RAM in the Linker-Script:  _siitcmram = LOADADDR(.itcmram); /* size of ITCM-RAM */ ....

CBerg by Senior II
  • 5354 Views
  • 12 replies
  • 3 kudos

compiler generating bad .elf file

Hello STM,I noted that the compiler generated a bad .elf file using an STM32H7R3L8H6H MCU. I made a small demo project(attachment) that demonstrated the problem.I'm using an external PSRAM with HEXASPI on XSPI1 port. I reserved a place on fixed addre...

Intector_0-1739248524203.png

STM32N6 Target not responding

Hello all,I'm working with the STM32N6-Discovery board on a camera application. I'm finding every so often when launching the debugger it will get a "Target not responding" error. Sometimes days go by where I can't debug my code until it randomly sta...

Resolved! STM32CubeIDE freeRTOS semaphore creation issue

Hi,I have a problem during creation of Semaphore in STM32CubeIDE. When I create a semaphore (dynamic or static) and add it to register view then.... nothing happens. I discovered that issue when in fact this mutex behaves as it wouldn't be created ev...

MarcinGajewski_0-1699617064869.png