STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1244 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 511 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! STM32F407 Breakpoint crossed-out

When i try to add breakpoint, there is a cross sign on breakpoint symbol. So even if the code works, breakpoint never works.I try to add __asm("BKPT 0"); but it also did not work. I am not sure what is the problem.My CubeID version is: Version: 2.1.1...

Resolved! How to generate a *.bin file instead of a *.elf file

hello ST Community,Is it possible to generate a binary file that is a *.elf file from a project developed by STM32CubeIDE?Using the correct settings for generating *.bin files.The *.bin file would be used to create a bootloader via UART for one of th...

Domy_ST by Senior
  • 376 Views
  • 4 replies
  • 3 kudos

stm32cubeide compilation speed issue

Hi, I'm using stm32cubeide version 2.1.1 and version 1.15.1/windows11, both are compiling the same project on my PC at slower speed compared to a lab computer.(3min vs 20seconds) Any idea what could be causing the issue? Thanks!

Resolved! NUCLEO-L452 STLink debugging external MCU using SWO

What could be the reason that configuring in CubeIDE SWV as enabled the MCU on debug flashes and stops responding? Flashing works fine both ways, SWO is connected. Time elapsed during verifying operation: 00:00:00.082Download verified successfullyTar...

KaLiO by Associate II
  • 331 Views
  • 2 replies
  • 0 kudos

Resolved! NUCLEO-U3C5ZI-Q project has no .ioc file

I'm trying to create an empty project for the NUCLEO-U3C5ZI-Q using STM32CubeIDE v2.1.1 under MacOS. All available updates have been applied.I've used File/STM32 Project Create to create an STM32CubeIDE Empty Project for the NUCLEO-U3C5ZI-Q board (al...

CTapp.1 by Senior III
  • 301 Views
  • 3 replies
  • 2 kudos

Include path in c++ Cube IDE

Hello,I am converting from Arduino to STM 32 Cube IDE. Here I have a Problem with include paths:What I want:- Develop Libraries in a special folder- Add the libraries as a LINK to the Cube IDE- use #include command to include the library into the pro...

Blinky Structure.png 2025-01-05 18_19_47-Properties for STM32_Blinky.png
DocAlex by Associate III
  • 2594 Views
  • 3 replies
  • 2 kudos

Resolved! st link debugging issue

hello team, I am facing a debug connection issue with STM32H723VGTx using STM32CubeIDE and ST-LINK.Issue details:MCU: STM32H723VGTxDebug tool: ST-LINK (OpenOCD via STM32CubeIDE)Interface: SWDReset mode: Software resetSWD frequency: 50 kHzObserved beh...

manoj3 by Associate II
  • 683 Views
  • 11 replies
  • 3 kudos