STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

Resolved! Change hardware target on STM32CubeIde

Apologies if this has been asked before, I did a search and couldn't find it.....Using STM32CubeIde, I set the project to be the USB dongle P-Nucleo-WB55. Now, trying to flash this and I am told it doesn't have debug capabilities. Shame, but OK, ther...

inky by Associate II
  • 5273 Views
  • 4 replies
  • 0 kudos

Can't upgrade RF stack...and can't upgrade...FUS...

Hello all, I'm currently stuck with the RF stack upgrade process a stm32wb55 nucleo board....i have follow the release notes in the "STM32WB_Copro_Wireless_Binaries" directory but i'm now out of idee to figure out what's going on...Currently i'm not ...

PJEAN.1 by Associate II
  • 4084 Views
  • 9 replies
  • 0 kudos

Resolved! Cant't find on Cube TSC peripheral for STM32WB55CEU

I'm start to develope a board with touch sensing capability using STM32WB55CEU 48 pin but is System Tab on CubeMX i can't find TSC peripheral.. cube is at 5.6.0 and FW package for STM32WB is 1.5.0Any suggestion?thanks in advance

0693W000000UuZbQAK.png
Pbern.11 by Associate
  • 1287 Views
  • 2 replies
  • 0 kudos

Does the STM32WB offer a wake up from RF feature?

I am looking for a controller that can operate on very low power and listen for RF messages. The RF message would wake up the controller. Is this possible on the STM32WB? I see that it can wake up from RTC events, but I do not want to rely on a timer...

CWill.1 by Associate
  • 1097 Views
  • 1 replies
  • 1 kudos

Turn off BLE temporary

Hey,in my application it should be possible to turn bluetooth on and off again completely.Turning advertising off, doesn't do the trick, because devices which have been paired before can still connect.Turning off the APB3 clock for BLE in the RCC_C2A...

How to Exten ATT MTU SIZE in the STM32WB55?

I use BLE_p2pServer application, and try to send long size data to Mobile APP (LightBlue) or Rpi4 application (bulepy ).I am only able to send 153 bytes for maximum.May I ask how to exten ATT MTU SIZE > 153 bytes in the STM32WB55?Thanks a lot.My code...

WWU.807 by Associate II
  • 812 Views
  • 0 replies
  • 0 kudos

p-Nucleo WB55, FUS ERROR IMAGE_NOT_FOUND

Hello, i'm using ST32 p-Nucleo WB55 and i'm trying to upgrade FUS, latest version. I 'm getting an error (FUS_IMAGE_NOT_FOUND) during the upload phase. This is the code:------------------------------------------------------------------- ...

FSara.1 by Associate II
  • 1122 Views
  • 1 replies
  • 0 kudos

Resolved! Micro sec delay with STM32L0

HiI am using a B-L072Z-LRWAN1  development board and I need to read data from a DTH22 sensor.I am trying to use TIM6 to get a micro second delay, but it seems I am missing something.The delay function :void delay (uint16_t time){ /* change your code ...

GErma.1 by Associate III
  • 1981 Views
  • 2 replies
  • 0 kudos