STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 221 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4066 Views
  • 0 replies
  • 3 kudos

Why I got verry low RSSI from P-NUCLEO-LRWAN1?

Posted on September 07, 2017 at 09:14I use a P-NUCLEO-LRWAN1 and I-cube-lrwan End_node firmware. It was connect with Semtech lora gateway but rssi is very low and it have some lose of message from P-NUCLEO-LRWAN1.  please see result a picture below....

0690X000006089PQAQ.png 0690X000006089UQAQ.png

STM32CubeExpansion_LRWAN_V1.1.1 uses stale L4 HAL

Posted on August 26, 2017 at 01:17The LRWAN tree contains a very old L4 HAL tree, doesn't support L496, also lacks support for NUCLEO 32 and 144 boards.Ported in the V1.8.0 L4 Cube supplied HAL libraries.Got about 90% through a port of the SX1272MB2...

0690X000006042FQAQ.jpg

Send LoRa packet with AT command - b-l072z-lrwan1

Posted on June 12, 2017 at 15:37Hello,I am trying to use LoRa connectivity with the brand new b-l072z-lrwan1 discovery board. The End Node project works perfectly but I have an issue with the AT Slave project. When I try to send LoRa packet to my Mu...

How can I process to Make a DFU OTA

Posted on August 02, 2017 at 09:02I'm currently working on a BLE device. This device has no screen nor keyboard. It is using a STM32L0 and is connected to an application on android.I want to make a DFU (device firmware update) via bluetooth (OTA) so...

STM32L072_Discovery

Posted on July 17, 2017 at 12:58Hi Support Team I am using STM32L072_Discovery kit..In cubeMx - Boards i am not able to see my board , i want to check power consumption for this board.Now i am manually checking using multimeter (i am using I2C , RTC...

Resolved! I-CUBE_LRWAN End Node does not work stably

Posted on May 05, 2017 at 09:34Hello.I try to use I-CUBE-LRWAN example End Node for stm32L152. Base station is iC880A with raspberry pi 3. Also i use https://community.st.com/discussion/thethingsnetwork.org. I ported this example to iM880B (stm32L15...

LoRaWAN demo DevEUI is not unique

Posted on June 29, 2017 at 18:12Hello,We've got two B-L072Z-LRWAN1 LoRa Discovery kit boards and we're trying to use the end_node demo project, included in the https://my.st.com/content/my_st_com/en/products/embedded-software/mcus-embedded-software/...

timer based sleep in ping pong

Posted on June 29, 2017 at 14:30Hi Support TeamI want to implement sleep mode in ping pong project , so slave device send some data and go to sleep  ..STM32L072CZYX - LORA DISCOVERY boardhow to put the device into sleep mode , please share some docu...

ping_pong_i2c_sensor

Posted on June 27, 2017 at 11:02Hi Support TeamQuestion 1 :I am using ping pong in ST-LORA discovery kit .I used cubeMx to generate code for reading i2c temprature/humidity sensor , it is working , here /** System Clock Configuration*/void SystemClo...