STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

STM32CubeIDE build problem

I downloaded these examples:https://github.com/ashkanr65/STM32CubeWB/tree/master/Projects/P-NUCLEO-WB55.Nucleoto follow them, but when I open these projects, I can't build them with my STM32CubeIDE.Anyone can help me?

ashkanr65 by Associate II
  • 17318 Views
  • 15 replies
  • 0 kudos

USB Dongle is "Unknow Device"

Hello, everybody! I faced with some problem. If I init USB_Device as CDC by STM32CubeMX then OS detect dongle as "Unknow Device", but if I use ready project from STM32Cube_FW_WB_V1.3.0 (BLE_TransparentModeVCP) then Dongle is working. What reasons of ...

0693W000000UMt8QAG.png 0693W000000UMtIQAW.png 0693W000000UMtcQAG.png

Resolved! STM32WBxx FUS seems to be deleted

Hi,I am currently working with the STM32WB Nucleo Boards. I wanted to flash a new FW on the Dongle. Therefore I enabled USB DFU Mode. I used the following command to write the new FW:$ ./STM32_Programmer.sh -c port=usb1 -w ~/Tools/STM32CubeWB/Project...

cyancali by Associate III
  • 10656 Views
  • 23 replies
  • 0 kudos

Wireless Stack Update via OTA bug

I am developing with the stm32wb nucleo kit, and I am testing the stBleSensor application, I have tried to update the Wireless Stack sending an erroneous file (pdf), and what happens is that it updates without problem and does not give any error, but...

AValt.1 by Associate II
  • 1799 Views
  • 3 replies
  • 0 kudos

STM32WB firmware update services question

Stumbling through the procedure described in app note AN5185 - ST firmware upgrade services for STM32WB Series using eval board MB1355C (STM32WB55). On page 3 of AN5185 it says:In order to check if FUS is running or not, the following options are a...

KSwee by Associate
  • 2394 Views
  • 5 replies
  • 0 kudos

Resolved! STM32WB55 BLE Stack trouble on new hardware

Hi All,I am having trouble getting the BLE working on my new hardware. As a base project, I am using the WB55 Nucleo BLE_DataThroughput application. My new hardware is using a STM32WBCEU6.Following the Release Notes in STM32Cube_FW_WB_V1.1.1/Projects...

0690X000009YojeQAC.png
Daniel L by Associate III
  • 7343 Views
  • 7 replies
  • 0 kudos

WB55 Nucleo: ST-Link causes MCU to reset randomly

I'm using an STM32WB55 Nucleo board. If I power and manage it via the built-in ST-Link USB interface, the result is very flaky. The CubeIDE debugger randomly loses its connection and, far worse, the MCU will randomly reset itself. When this reset ...

David C. by Associate II
  • 3575 Views
  • 6 replies
  • 0 kudos