STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 228 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4071 Views
  • 0 replies
  • 3 kudos

STM32WB55 TSC is not working

In Group 1 G1_IO4 is a sampling capacitor and G1_IO3 is a sheild and in Group 2 G2_IO2 is sampling capacitor and G2_IO1 is input touch key. In Group 3 G3_IO4 is a sampling capacitor and G3_IO2 is a input touch key. so when i programmed with this conf...

Smalik by Associate II
  • 1658 Views
  • 3 replies
  • 0 kudos

Resolved! Repeated write SD RAM + reset

Hello, I'm working on STM32WB55.Is there any limitation to write to (internal) SD RAM and do a system reset?I want to build an application that requires a lot of writing to SD RAM and then do system reset (and read the SD RAM and act according the da...

Lmali.1 by Associate III
  • 1583 Views
  • 2 replies
  • 0 kudos

hello sir, am porting some libraries done in stm32l4 board to stm32wb board and linked some provided libraries to stm32 wb board but in the end it shows some error 1 message without any clue.Please, Can you help me out in this ?

arm-none-eabi-gcc -o "P2P_Server.elf" @"objects.list" -lbep_diag_hf -lbep -lbep_diag -lbep_hf -mcpu=cortex-m4 -T"D:\kiran\new1\p2p\P2P_Server\P2P_Server\STM32CubeIDE\STM32WB55RGVX_FLASH.ld" --specs=nosys.specs -Wl,-Map="P2P_Server.map" -Wl,--gc-secti...

Pratyush by Associate II
  • 966 Views
  • 1 replies
  • 0 kudos

Resolved! STM32WB USART1 not working

Hello, please be warned, I am ultra new to STM32 mikrocontrollers (student).I watched several hours of tutorials and now I am starting my first steps in programming. I am using the CubeMX to set up the code.Unfortunately, I can´t get the USART1 runni...

RWeil.2 by Associate III
  • 3224 Views
  • 2 replies
  • 1 kudos

P-NUCLEO-LRWAN2 issue

Hello,I am currently testing the P-NUCLEO-LRWAN2. I am having problems getting it to work. I followed the tutorial in the UM2073. I managed to perform all the steps requested but I don't receive any data in the LORIOT dashboard.I also uploaded the "E...

MChar.1 by Associate II
  • 641 Views
  • 0 replies
  • 0 kudos

Resolved! STM32WB55 Cube MX 5.6 Generated Code Errors

When using the Custom Template option in Cube MX 5.6 for the WB55, the generated "custom_stm.c" file contains some bugs in the "Custom_STM_App_Update_Char" function. Namely, the calls to "aci_gatt_update_char_value" mistakenly pass the characteristic...

BPaik by Senior
  • 2993 Views
  • 5 replies
  • 0 kudos

B-LO72Z-LRWAN1 HAL_RNG

HiI am trying to generate a true random number on the B-LO72Z-LRWAN1 using the HAL_RNG_GenerateRandomNumber function with the code below:uint32_t rnd_generator (void) {RNG_HandleTypeDef RngHandle;  // RNG handler declaration uint32_t rv;  RngHandle.I...

GErma.1 by Associate III
  • 1583 Views
  • 1 replies
  • 0 kudos