STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 222 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4067 Views
  • 0 replies
  • 3 kudos

Resolved! STM32WB55 BLE OTA Process Issue

Using STM32CubeMonitor-RF I am able to update my device via OTA with one small issue. I send the command to program my device and my application gets deleted and the device reboots into our OTA application but I have to search for my device a second ...

0693W000003Ph5kQAC.png 0693W000003Ph6EQAS.png

Radio Peripheral Documentation

STM32WB SoCs have radio module. I need a way to write own wireless stack but the documentation is lacking their description.So far documentation mentions 3 peripheral devices on APB3:0x6000 1000 - 0x6000 1FFF 4 KB 802.15.4 CTRL0x6000 0400 - 0x6000 07...

Teivaz by Associate
  • 3336 Views
  • 12 replies
  • 0 kudos

STM32WB sequencer bug?

Hi,I'm using CubeMX to generate the code for the STM32WB and I found a problem in the secuencer library which is automatically generated.When I register a new task in the scheduler, this places the callback function in TaskCb[0] but when I set the ta...

Diego B. by Associate II
  • 2726 Views
  • 4 replies
  • 0 kudos

B-L072Z-LRWAN1 with sleep-on-exit feature

Hi there, I'm using a customized board based on B-L072Z-LRWAN1. I also use I-CUBE-LRWAN (v1.1.4), compiled on Keil uVision. Everything works fine. I can get about 2uA in Stop mode. Now I'm doing a project requiring power consumption optimized so I en...

JLe.1 by Associate
  • 1056 Views
  • 1 replies
  • 0 kudos