STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 222 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4067 Views
  • 0 replies
  • 3 kudos

PIN FUNCTIONS IN MURATA LORAWAN MODULE

HiAccording to the Murata's manual, the CMWX1ZZABZ-091 module uses an STM32L082 processor, but the ST website says it uses an STM32L072CZ. What information is correct?I am asking this question because the Murata manual does not reference all the alte...

GErma.1 by Associate III
  • 4259 Views
  • 8 replies
  • 0 kudos

Device Information Table is validity

AN5185 lists the contents of the device information table in Table 5What information in this table is valid at which state (wireless stack running or FUS running) of CPU2?My initial guess was that it should be valid during FUS execution as well as Wi...

HRadt.1 by Senior
  • 1365 Views
  • 3 replies
  • 0 kudos

Simple Bluetooth Client Examples

Is there any public examples of a stm32wb Bluetooth client application. Where the stm32wb client does a few read's and write to a server bluetooth applicaion. What i was thinking of was a BLE_HeartRate_Client program to the BLE_HeartRate program ...

Badam.17 by Associate II
  • 902 Views
  • 0 replies
  • 0 kudos

STM32WB55 TSC is not working

In Group 1 G1_IO4 is a sampling capacitor and G1_IO3 is a sheild and in Group 2 G2_IO2 is sampling capacitor and G2_IO1 is input touch key. In Group 3 G3_IO4 is a sampling capacitor and G3_IO2 is a input touch key. so when i programmed with this conf...

Smalik by Associate II
  • 1645 Views
  • 3 replies
  • 0 kudos