NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi, I wanna use STM32WL for 148-152Mhz. But I cannot out 13dBm power for RFO_LP.If anyone know Zopt impedance for 150MHz ins this IC, you let me know it. Off course 169MHz is no problem. Almost of application note is written over 433MHz.Thanks.
Is it possible to integrate BLE OTA functionalities into BLE LLD projects? For example, we would like to make the BLE_LLD_Proximity example OTA compatibile, which however requires the FW stm32wb5x_BLE_LLD_fw.bin, while the BLE Ota bootloader example ...
Is it possible to write a custom co-processor binaries for CPU2 instead of using the coprocessor binaries from stm
Hello,I am using p2p_server BLE example with RTC Internal Wakeup with interrupt. But somehow void RTC_WKUP_IRQHandler(void) is not getting called. Please let me know the possible reason.Regards.
Hello dear tech support and comunity.Is it possible to get sources for ST BLE Sensor 4.12.0 for Android and were?Here https://github.com/STMicroelectronics/STBlueMS_Android it seems to be only 4.9.0 as latest one.BRAlex
when the example file is modified but the original program gets recovered when the Device Configuration Tool Code Generation is hit after some changes in ioc file.#stm32wl55jcIts hard to start from the scratch in LoRa subghz, Do anyone have some meth...
I am Attaching Observed Current Consumptions. I am observing Huge Difference between claimed current value versus observed current value at various low power modes. I am having right Connections as mentioned in Power Consumption measurement board Dat...
I'm trying to run broadcasting mode on the base off BLE_P2PServer example and instead of aci_gap_set_discoverable in app_ble.c, in "Adv_Request" function, I'm trying to use the below function: aci_gap_set_broadcast_mode( Min_Inter, Max_Inter, ADV_NO...
How much flash memory is allocated for CPU2 flash and is it possible to write a RF firmware without involvement of CPU2