2021-01-11 5:07 AM
I have created a board based on STM32WB55CG which is same microcontroller as that is used in P-NUCLEO-WB55.USBDongle.
The problem is, in STM32Cube_FW_WB_V1.10.0 project folder for P-NUCLEO-WB55.USBDongle board, there is no BLE_MeshLightingProvisioner example included.
I have tried to read AN5292 document, but there is nowhere this is mentioned on how to port project from one microcontroller to another.
Also, i have noticed that, the Upper Tester protocols as explained in AN5292 using the provided project BLE_MeshLightingPRFNode are not working either but everything else works; something to do with command not being sent to microcontroller using the VCOM port.
Can anyone help on this?