cancel
Showing results for 
Search instead for 
Did you mean: 

Dificulties with the I-NUCLEO-LRWAN1 aka WM-SG-SM-42

CSilv.1
Associate

Im trying to use the STM32 Nucleo Pack LoRa HF band sensor and gateway, and im trying to program the I-NUCLEO-LRWAN with the firmware, but im getting no responde from the shield. I did a little bit of research and found out about the firmware update that you can do, but every time i try to run the program, with the conections provided by the guide, the program doesn't open. Do you need to run de SWD connection + UART or only one of the two? Plus, since i tried to run the sm42_backup program, the shield doesn't even light up anymore when i plug it in.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
ANauz.1
Senior II

Hello,

You should try any other solution but I-NUCLEO-LRWAN1 aka WM-SG-SM-42!!

I had one who was responding, and try to update it with a new firmware. After no succes, the board do not answer any more to any request.

I try to get support from USI by email and by sending message on there Github! No response at all!!

Client support is really nonexistant here!! To bad!!

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.