cancel
Showing results for 
Search instead for 
Did you mean: 

I also want to stop M0 + and RF in order to minimize the power consumption when SLEEPing STM32WB.

MNitt.1
Associate II

I would like to completely stop M0 + and RF in order to minimize power consumption when SLEEPing STM32WB. Is such a thing possible? I tried various things with reference to the sample code and documentation, but M0 + / RF did not seem to be stopped.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
TGUCL.1
Associate III

Hi

Did you get anywhere with this ? I`m having the similar problems. If I use p2pserver on usb dongle current consumption is about 14-15 mA which is huge.

MNitt.1
Associate II

Hi, TGUCL1 Mr.

It went well. I don't know if it's the original method, but I was able to reduce the power consumption by stopping the Radio Clock and then Deep Sleeping M0+.