NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello,I am developing a project that includes a bootloader and an application to jump to.Both binaries execute on the M0+ core in order to take advantage of the security features offered only for this core.The idea is as follows:The bootloader verifi...
Hello, I bought this development kit to learn LoRaWan technology and improve myself.P-NUCLEO-LRWAN2STM32 Nucleo pack LoRa™ HF band sensor and gateway.I made the connections of the product as written in the User's Manuals and saw that the product was ...
Sir, I testing the STM32L0 + SX1276 with en.i-cube_lrwan_v2.1.0 libI compiled the AT COMMANDS example on KEIL and then with STM32 IDE too, but during execution i am always getting the following error in bothAPP_VERSION: V1.1.0MW_LORAWAN_VERSION: V...
It is possible to share the schematic and BOM files of the MB1552B board presented as a design reference in the document: "AN5407 Optimized RF board layout for STM32WL Series" ?
Will ST Micro pursue that certification on the module/SOC level? Or will vendors have to pursue that certification independently/at the device level?
Hello,I'm looking for some example code on using the built in RTC for the STM32WB55 to get a timestamp in UNIX UTC Time in milliseconds. Or the number of milliseconds since January 1st 1970.If anyone has a simple example on how to accomplish this I w...
Good morning......I am using the ADC with 2 channels (Ch 9 and Ch 10). I am using an LPTIM to take these samples every 15ms. I have the ADC callback (HAL_ADC_ConvCpltCallback) to interrupt on 'End of sequence of conversion' (per .ioc --- or so I thin...
We have encountered issue with WB55 BLE firmware where it doesn't accept AD_TYPE_COMPLETE_LOCAL_NAME longer than 9 characters We have reproduced that issue on p2pServer example where we've modified local_name to be "123456789" all is OK.static const ...