Browse
STMicroelectronics Community
FAQs
Sign In
Product forums
STM32 MCUs
STM32 MCUs products
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
STM32 MCUs Other solutions
STM32 MPUs
STM32 MPUs products
STM32 MPUs Boards and hardware tools
STM32 MPUs Software development tools
STM32 MPUs Embedded software
STM32 MPUs Solutions
MEMS and sensors
MEMS (sensors)
Imaging (sensors)
Automotive & Transportation
Microcontrollers
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
HAgar.1
Associate II
since
2021-06-05
2023-06-14
User statistics
12
Posts
0
Solutions
0
Kudos given
0
Kudos received
View all badges
STMicroelectronics Community
About HAgar.1
Options
Report User
User Activity
Posts
Replies
I want to connect HC-05 Bluetooth Module to STM32WB30 MCU. Are specific pins required or any GPIO will work to connect the module? Also is there any reference design for the STM32WB30 MCU?
2021-07-22
What values of pull-up resistors should be used for the BOOT0 and BOOT1 pins in the STM32WB30CE MCU? They are not mentioned in the datasheet for the MCU.
2021-07-10
I want to power my STM32WB30 MCU from a coin cell. Can anyone provide me with a circuit of some sort to do so. I am beginner with this and don't have any testing equipment to test the circuit so a circuit or schematic would be really helpful.
2021-06-21
Can we use external capacitors with the 32MHZ HSE instead of the programmable internal capacitors in STM32WB30CE MCU? If no, then how are the internal CAP programmed.
2021-06-05
Re: What values of pull-up resistors should be used for the BOOT0 and BOOT1 pins in the STM32WB30CE MCU? They are not mentioned in the datasheet for the MCU.
2021-07-25
Okay, I have seen that 100Kohm is also used in some MCU, so will there be any difference when using 10K or 100K?
Re: I want to connect HC-05 Bluetooth Module to STM32WB30 MCU. Are specific pins required or any GPIO will work to connect the module? Also is there any reference design for the STM32WB30 MCU?
2021-07-22
Okay Okay, I can only see USART in the STM32WB30 pin description. I can use them right? I do not know much about USART or UART so I am really confused.
Re: I want to connect HC-05 Bluetooth Module to STM32WB30 MCU. Are specific pins required or any GPIO will work to connect the module? Also is there any reference design for the STM32WB30 MCU?
2021-07-22
Okay so if I want to connect with hardware, does it mean I have to use the pins with USART?
Re: I want to connect HC-05 Bluetooth Module to STM32WB30 MCU. Are specific pins required or any GPIO will work to connect the module? Also is there any reference design for the STM32WB30 MCU?
2021-07-22
.
Re: What values of pull-up resistors should be used for the BOOT0 and BOOT1 pins in the STM32WB30CE MCU? They are not mentioned in the datasheet for the MCU.
2021-07-11
That's the issue, they are not mentioned in the datasheet for this MCU
View more