STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 220 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4065 Views
  • 0 replies
  • 3 kudos

Resolved! Cant power B-L072Z-LRWAN1 with battery

We recently received our B-L072Z-LRWAN1 but are not able to run the program while batteries are plugged in. In the datasheet it says that we need to remove SB37 to accomplish this. But then I cant program it anymore? How can I use the board with batt...

KPage by Associate
  • 14097 Views
  • 26 replies
  • 1 kudos

Resolved! STM32WB55 color control cluster gives an assertion error. assertion "zigbee_app_info.colorControl_server_2 != NULL" failed.

As I said, I get the assertion "zigbee_app_info.colorControl_server_2 != NULL" failed error from a standard debug function in the code.I thought it could have something to do with this struct, which is a bit above it.struct ZbColorClusterConfig color...

STM32WL55CC LPUART1 to UART1 freeze

Hello everyone,I work on a project with LSM100A whitch integrate an STM32WL55CC.I have an SDK available to start development and in this SDK, we can find debug information on LPUART 1 (PA2,PA3).For my project, i can't use LPUART1 so i have decided to...

MLam by Associate III
  • 1792 Views
  • 2 replies
  • 0 kudos

Output Compare Interrupt on TIM16 STM32WB55

I am trying to use CubeMX to set up an Output Compare Interrupt on TIM16 of STM32WB55. I do not want anything to go to an output pin I just want to generate an interrupt....Can someone tell me where I set the switch that allows this interrupt as I d...

SWenn.1 by Senior III
  • 1558 Views
  • 3 replies
  • 0 kudos

Resolved! Bluetooth classic profiles (SPP / A2DP) on STM32WB

Hello,I have experience using Bluetooth classic profiles: SPP and A2DP.Started using STM32WB and I understand it doesn't support these two above profiles, it only has a stack for BLE. Is this correct?Can I use STM32WB with SPP and/or A2DP, if yes - h...

JUker by Associate II
  • 13476 Views
  • 13 replies
  • 1 kudos

Stm32WB55 custom board RF part error.

Hello, I have been testing my custom board using MCUs, Stm32WB series, these days.Actually, I successfully opened my own custom board with a functioning RF part (BLE).However, there is still an undeclared issue with new WB MCUs.When I used a new WB M...

WPARK.1 by Associate III
  • 4727 Views
  • 8 replies
  • 0 kudos