User Activity

Dear STM32WL community,I have completed a port of the ST LoRaWAN_End_Node application for use on the STM32WLE5XX as implemented on the RAK Wireless RAK3172 and SEEED Studios LoRa-E5 modules. It is based on the LoRaWAN_End_Node example in the latest (...
Hello,I am having problems with stm32wle5xx interrupt servicing. When an interrupt occurs, the M4 seems to jump to an arbitrary location and not the location in the vector table. I observe this only on the stm32wle5xx (on a RAK31772 module), and not ...
In ST's documentation, great pains seem to be taken to avoid specifically identifying the Semtech SX126x radio implementation. ST consistently refers to it as a "sub-GHz radio." Why is this?
Same issue as @PK.3 (but I would like the response to be shared with the community  ) : using a 4 volt OC 425 mA SC series photovoltaic, and SPV1040 with circuit matching STEVAL-ISV006V2 except Rs = 0 ohms and no VR4 (https://www.st.com/content/ccc/...
Kudos from