stm32wle5xx interrupt failure
Hello,
I am having problems with stm32wle5xx interrupt servicing. When an interrupt occurs, the M4 seems to jump to an arbitrary location and not the location in the vector table. I observe this only on the stm32wle5xx (on a RAK31772 module), and not on the stm32wl55xx (on a nucleo-wl55jc development board).
Specifically, I wrote a very simple STM32CubeIDE project which loops waiting for an EXTI15_10_IRQ interrupt when PA15 is pulled low. The loop waits 10 seconds after reset before enabling EXTI15_10_IRQ. If I do not pull PA15 low, the loop runs forever. If I pull PA15 low, before EXTI15_10_IRQ is enabled, the loop runs until the interrupt is enabled at 10 seconds, then jumps to a nonsense location. If I pull PA15 low after the interrupt is enabled, then the processor jumps immediately to the nonsense location.
I have verified that the interrupt vector table is correct (specifically, address 0x080000E4, the address of the EXTI15_10 vector) has the correct address for the handler.
Note that this behaviour occurs with ANY interrupt, not only the EXTI15_10 interrupt. I just chose this one to work on because it was very simple.
Any ideas? Remember, the exact same code (.bin file) works properly on the STM32WL55xx on the nucleo-wl55jc but fails on the STM32WLE5xx on the RAK3172.
Thank you!