User Activity

I'm not able to pair our application running STM32WB55 via STM32CubeMonitor-RF. Pairing with iOS sniffer apps are working. What are the settings and commands I shall apply in STM32CubeMonitor-RF?Our device is using a 6 digit pin, bondle mode, MITM pr...
I can't read more then 8 bytes long attribute value from BLE characteristics with P-NUCLEO-WB55.USBDongle from STM32WB55. It might be a bug?Details:I have 4 characteristics in my service. I can read the first 3 characteristics with ACI_GATT_READ_USIN...
I can read characteristic value in P-NUCLEO-WB55 based application with ACI_GATT_READ_USING_CHAR_UUID command. However, I do not find any command for subscribe for notification (AN5270 docs neither STM32CubeMonitor-RF ACI commands). How can I subscri...
I tried to update the firmware on P-NUCLEO-WB55 devboard, but it fails with the following error:"Error: FUS_STATE_ERR_UNKNOWNError:Old Firmware delete failed"I check in STM32CubeProgrammer, and I have V.0.0.0 version: I do not know why it happened, m...
I checked I2C interrupt flags, when I realized at new interrupt bit 16 is also checked for SR1, bit 17 is also checked for SR2 registers, despite they are 16-bit registers. Why? See attached picture for details.Thanks in advance!
Kudos from
Kudos given to