STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 159 Views
  • 0 replies
  • 0 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4035 Views
  • 0 replies
  • 3 kudos

NucleoF411 and IDB05A2 BLE beacon message reading?

Hello!I would like to ask for some help in my STM32 Project.In this project I want to receive and process a BLE beacon message with a Nucleo F411 board and X-Nucleo-IDB05A2 Bluetooth Shield.The message came from a simple device without any in or out ...

PPall.2 by Associate II
  • 1757 Views
  • 3 replies
  • 0 kudos

STM32WB55RGV6 (board P_NUCLEO_WB55) STM32cubeprogrammer errors show: first erro: No STM32 target found when i press button 'reset' error: ST_link erro(DEV_TARGET_CMD_ERR) stm32cubeide errors: error in launch sequence: Failed to startGDB server

Note: I can use stlink to download programs to other boards.But p_nulceo_wb55 doesn't work well. I use an external stlink instead of the on-board stlink, the errors are same.I was learning Bluetooth, It would have worked well. After a while, an erro...

0693W00000NpzZQQAZ.png 0693W00000Npzb7QAB.png
Lep by Senior
  • 3666 Views
  • 10 replies
  • 0 kudos