STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

Resolved! RTOS Proxy driver port for STM32WB55

I want to enable the RTOS Proxy in the debug launch configuration for my STM32CubeIDE project. However, in the "Driver settings" fieldset, I need to select a "Port" from a dropdown. The options in that dropdown confuse me. I have an STM32WB55, which ...

LWChris by Associate III
  • 3019 Views
  • 4 replies
  • 3 kudos

Smart Card communication baud rate error.

Hello, We're using STM32WB55RGV6 and trying to communicate with a smart card. At the beginning of communication, we can read ATR and we can send and receive PPS successfully. But when we try to send an APDU message our data signal doesn't fit our cal...

0693W00000SvTjQQAV.png

Launch FUOTA in custom application for a STM32WB5MMG

Hi,I'm currently working to start the FUOTA on a STM32WB, so I've spent several time following the Application Note AN5247 and watching the MOOC - STM32WB Firmware Update Over the Air (FUOTA) videos that explain how to run the OTA on a P-NUCLEO-WB55 ...

jorgazam by Associate II
  • 1611 Views
  • 1 replies
  • 0 kudos

Erasing of flash in STM32WB BLE OTA example not working

I have loaded BLE OTA example (v1.13.1) to my STM32WB50CG. User application starts on default set address 0x08007000. Problem is when I send a BLE command to OTA Reboot characteristic (to load into OTA, first sector + how many to delete) from my Andr...

tj.1 by Associate
  • 1302 Views
  • 1 replies
  • 0 kudos

Resolved! Does the STM32WB55RGVx support DTM over UART?

According to BLUETOOTH CORE SPECIFICATION Version 5.3 | Vol 6, Part F, there are two methods of supporting DTM: DTM over HCI and DTM trough 2-wire UART. I know that WB55 supports DTM over HCI for sure, but what about DTM over 2-wire UART? It's also s...

STM32 with Ebyte Lora

Hi everyone, I am a student and I used arduino for now. I have stm32f4 disocvery board, stm32f103c8t6 and stm32f401ceu6. I have lora module E32-44t30D module which is working with UART. I was using these with arduino and there is a lot of library for...

anone.1 by Associate
  • 2321 Views
  • 0 replies
  • 0 kudos