STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 219 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4065 Views
  • 0 replies
  • 3 kudos

How to properly add a task to LoRaWAN_End_Node

Hello everyone,​Situation: Currently, I am trying to intergrate BME688 to the board Nucleo-WL55JC1. To be specific, on the board, I downloaded and ran the LoRaWAN_End_Node example. Then, instead of obtaining temperature/humidity/pressure from a funct...

HNguy.25 by Associate III
  • 2558 Views
  • 2 replies
  • 1 kudos

Connecting STEVAL-PROTEUS1 to a pre-existing thread network

I'm currently working with the "Thread_Coap_Generic" example for the STM32WB, which I got from MXCube. I want to connect to a pre-existing thread network. I have changed the panid and channel of the example to that of my network (in the "app_thread.c...

BBI Louw by Associate
  • 892 Views
  • 0 replies
  • 0 kudos

Resolved! difference between WL55JC1 and WL55JC2 versions of Nucleo

https://www.st.com/en/evaluation-tools/nucleo-wl55jc.html indicates that it has "Arm® Cortex®-M4/M0+". I am confused about this: does it use an M4 or an M0+?Also, what is the difference between the WL55JC1 and WL55JC2 versions of the Nucleos? Please ...

JGree.16 by Associate II
  • 2215 Views
  • 3 replies
  • 0 kudos

Resolved! I2C implementation based on freeRTOS OS

Hello,I'm using STM32WB55 in conjunction with freeRTOS OSI found a very good I2C BARE-METAL working example located at:..\STM32Cube\Repository\STM32Cube_FW_WB_V1.12.1\Projects\P-NUCLEO-WB55.Nucleo\Examples\I2C\I2C_TwoBoards_AdvComITI'm looking for a ...

Resolved! Can not connect to STM32WB via ST-Link

Hello, I many years used ST-Link to download my framework to STM32, so I am not new in this.But now - I used all available settings in - ST-LINK software (under reset, hot, normal, with different frequency). I pushed reset in the boards, I connected ...

0693W00000UFRICQA5.jpg 0693W00000UFRIRQA5.jpg
IRakh.1 by Associate III
  • 5331 Views
  • 11 replies
  • 0 kudos

STM32WLE5CBU6 LoRa TxTimeout

Hi,I created Lora project which send and receive data. I designed my board, no TCXO.My schematic:My result:the random value is 0, TxTimeout everytime.I replaced to new MCU, new RF switch IC but result not change. Please support me.Thanks.

0693W00000UFQ6yQAH.png 0693W00000UFQ2IQAX.png

Resolved! FatFs cannot write file larger then 64kB

Hi i build an application with fatfs implementation to log data.but when the file size reach 64kB, the SD card stop responding and i can not write on it.I used standard configuration for ff_confany suggestion to resolve the problem ?thank you.

malarab by Senior II
  • 3099 Views
  • 3 replies
  • 0 kudos