STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 221 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4067 Views
  • 0 replies
  • 3 kudos

STM32WLE5 frequency deviation for FSK modulation

Greetings,what is the recommended frequency deviation parameter for the FSK modulation with 250 kbps bitrate?Or rather what is the dependency of RX sensitivity in relation to the FSK_FDEV parameter?I can see that the limitation is to have the modulat...

DTomi.1 by Senior
  • 2325 Views
  • 1 replies
  • 0 kudos

Resolved! LoRaWAN_End_Node: varying configuration

Hello everyone,I am now working with LoRaWAN_End_Node on Nucleo-WL55JC1 and I found no place to change configuration such as BW, TX power, Spreading Factor, etc. in this example (Probably, I found at wrong places).Is it possible to change those facto...

HNguy.25 by Associate III
  • 2906 Views
  • 6 replies
  • 0 kudos

How can i start ble project with nucleo-wb15cc???

Follow Lecture : WB Bluetooth mesh - 7 Lab 1: Creating Bluetooth Low Energy project STM32WBMMG-DKHello, I am a student who recently started the low power Ble project.I bought a nucleo-wb15cc board and am working on the project. After reading this lec...

remoter by Associate III
  • 1715 Views
  • 3 replies
  • 0 kudos

stm32wb55 avoid exit from sleep mode with TIM2 is active

Hello everybody, I am working with a stm32wb55 and in my application I need to send the microcontroller to sleep for 5 second, wake up, perform some actions and go back to sleep.I send the micro to sleeomode using the function  HAL_PWR_EnterSLEEPMode...

AFede.1 by Associate
  • 1416 Views
  • 1 replies
  • 0 kudos

Pairing Authentication for Client (Centaral) side

What parameters of 'aci_gap_set_authentication_requirement' are relevant for client side?What can I set the irrelevant parameters to?tBleStatus aci_gap_set_authentication_requirement( uint8_t Bonding_Mode, ...

DS.4 by Senior II
  • 1067 Views
  • 1 replies
  • 0 kudos

Resolved! Trouble exporting BLE server from Nucleo to custom board.

Hello,Working on a custom BLE server (peripheral role), I face a trouble exporting the working sources from a Nucleo project (STM32WB55) to a custom board (STM32WB55) project.Everything is working fine on the Nucleo: advertissing, connection, bidirec...

Mickael1 by Associate II
  • 2353 Views
  • 3 replies
  • 0 kudos